THICKNESS VERIFICATION OF MPC860TCVR50D4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

THICKNESS VERIFICATION OF MPC860TCVR50D4

2,122 Views
IGH0209
Contributor I

Hi,

 

I have purchased MPC860TCVR50D4 from the vendor recently. When I checked the part, thickness was different as below. 

 

Thickness (should be)  : 2.5MM ZQ/VR PACKAGE

Thickness (current) : Assumed 1.77MM ZP PACKAGE

 

When I checked the thickness it is 1.81mm, but I don't see that thickness from the website. (It only shows body 25 x 25 x 2.52mm) 

 

Vendor advised me that it is BGA357 Package and it was a newer version which might be thinner for energy efficiency. I would like to verify from you if it is correct. 

 

Thank you,

Chris Park

Tags (1)
0 Kudos
Reply
0 Replies