THICKNESS VERIFICATION OF MPC860TCVR50D4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

THICKNESS VERIFICATION OF MPC860TCVR50D4

2,125件の閲覧回数
IGH0209
Contributor I

Hi,

 

I have purchased MPC860TCVR50D4 from the vendor recently. When I checked the part, thickness was different as below. 

 

Thickness (should be)  : 2.5MM ZQ/VR PACKAGE

Thickness (current) : Assumed 1.77MM ZP PACKAGE

 

When I checked the thickness it is 1.81mm, but I don't see that thickness from the website. (It only shows body 25 x 25 x 2.52mm) 

 

Vendor advised me that it is BGA357 Package and it was a newer version which might be thinner for energy efficiency. I would like to verify from you if it is correct. 

 

Thank you,

Chris Park

タグ(1)
0 件の賞賛
返信
0 返答(返信)