T1042 JTAG select

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1042 JTAG select

1,891 次查看
shinbo
Contributor II

What is the JTAG of T1042?

0 项奖励
回复
3 回复数

1,880 次查看
nxf45548
NXP Employee
NXP Employee

Hi @shinbo 
Thank you for contacting NXP technical support. 
You can use the JTAG the Codewarrior Tap: 
https://www.nxp.com/design/software/development-software/codewarrior-development-tools/run-control-d...

Regards, 
Susi

0 项奖励
回复

1,876 次查看
shinbo
Contributor II

It is confirmed that CW_TAP is JTAG.
Then, I want to build RCW file on T1042, what file should I build?
ex) .bin, .elf

1,702 次查看
Hector_Villarruel
NXP TechSupport
NXP TechSupport

If you are trying to load code from the beginning you probably need the .elf file.

On the other hand whether you are trying to load an specific application or using some codes that the main code use in his place, you will need the .bin file

Best Regards,

Hector Villarruel

0 项奖励
回复