T1042 JTAG select

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 JTAG select

1,894 Views
shinbo
Contributor II

What is the JTAG of T1042?

0 Kudos
Reply
3 Replies

1,883 Views
nxf45548
NXP Employee
NXP Employee

Hi @shinbo 
Thank you for contacting NXP technical support. 
You can use the JTAG the Codewarrior Tap: 
https://www.nxp.com/design/software/development-software/codewarrior-development-tools/run-control-d...

Regards, 
Susi

0 Kudos
Reply

1,879 Views
shinbo
Contributor II

It is confirmed that CW_TAP is JTAG.
Then, I want to build RCW file on T1042, what file should I build?
ex) .bin, .elf

1,705 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

If you are trying to load code from the beginning you probably need the .elf file.

On the other hand whether you are trying to load an specific application or using some codes that the main code use in his place, you will need the .bin file

Best Regards,

Hector Villarruel

0 Kudos
Reply