T1024 - core clock frequency speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 - core clock frequency speed

Jump to solution
3,144 Views
giacomo_gaspari
Contributor II

Hi,

due to chip shortage we'll have to evaluate T1024NSE7PQA (F_core_clk=1400MHz) instead of actual T1024NSE7KQA (F_core_clk=1000MHz).

From the manual it seems that using the alternative chip would be possible without changing any RCW or other FW/HW data.

Could you please confirm my hypothesis?

Labels (1)
0 Kudos
Reply
1 Solution
3,139 Views
ufedor
NXP Employee
NXP Employee

Your understanding is fully correct.

The 1400 MHz part can be used in place of the 1000 MHz part without any change in hardware and firmware.

View solution in original post

1 Reply
3,140 Views
ufedor
NXP Employee
NXP Employee

Your understanding is fully correct.

The 1400 MHz part can be used in place of the 1000 MHz part without any change in hardware and firmware.