T1024 Absolute maximum ratings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1024 Absolute maximum ratings

958 Views
kojimiura
Contributor III

The maximum rating of DVIN of DUART is 'GND to (DVDD x 1.1)'
Is it safe to interpret the maximum rating of DVDD as 3.6V x 1.1 = 3.96V regardless of the power supply

voltage of DVDD?

Thank you.

 

0 Kudos
Reply
0 Replies