Supported codewarrior IDE version for the MPC860

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Supported codewarrior IDE version for the MPC860

2,300 次查看
maheshwarreddy
Contributor I

Now we are using the MPC860 power Quicc processor . we had installed the codewarrior 10.5.1 but we are unable to find the MPC860 series device .which version of the codewarrior we need to install . 

标记 (3)
0 项奖励
回复
2 回复数

2,185 次查看
Pavel
NXP Employee
NXP Employee

Use CodeWarrior 8.8 classic edition for the MPC860. See attached snapshots.

 

This CodeWarrior is available using the following link:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,185 次查看
maheshwarreddy
Contributor I

Thank you for the reply .

I had installed the code warrior v8.8 while installing the code warrior we are getting the error as cannot run an x86 buit of this utility on x64 platform .How to solve this issue.

Thank you 

Best regards

Maheshwar

0 项奖励
回复