Spurious I2C Interrupts on MPC8349E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Spurious I2C Interrupts on MPC8349E

1,217 Views
dijo
Contributor III

We have a board with MPC8349E running with VxWorks 5.5.
We got a sporadic (1 time, not reproducible) issue whereby we got a plethora of I2C1 interrupts which caused a kernel workQ panic.


In a usual run, we never get these interrupts, and we never expect it to come.
How do we continue to debug this issue? Could it be that i2c controller somehow got into a bad shape? What info can help to further debug?


Thanks

Dijo

0 Kudos
Reply
2 Replies

1,048 Views
alexander_yakov
NXP Employee
NXP Employee

For I2C module interrupt reasons and interrupt processing flowchart please look MPC8548E Reference Manual, Table 11-7 and Figure 11-11.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,048 Views
dijo
Contributor III

Thanks Alexander. On checking our isr code, I could see that the branch on

the right (i.e. I2CCR[MSTA] == 0 and following tree) is not implemented.

Could you help in understanding the impact?

Thanks.

On 4 June 2014 09:08, alexander.yakovlev <admin@community.freescale.com>

0 Kudos
Reply