Software Emulation Exception

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Software Emulation Exception

跳至解决方案
6,069 次查看
phani
Contributor I

Hi ,

 

I am getting the Software Emulation Exception exception while executing the code in MPC860T am using the code warrior 8.1.am getting the exception when ever i start executing from __start am getting exception while executing

 

mr r14,argc

mr r15,argv

mr r16,envp

 

If there is any mistake in the __start file plese let me know.

Original Attachment has been moved to: __start.c.zip

标签 (3)
标记 (1)
1 解答
5,583 次查看
alexander_yakov
NXP Employee
NXP Employee

The root cause of this problem is in some sensitive registers corrupted during initial device initialization before entering this __start subroutine.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
5,583 次查看
ravadasrikanth3
Fresh Out Contributor

Hi phaneesh,

we are also facing the same issue software emulation exception can you suggest how to solve the issue and the configuration file looks same as you were used with 66Mhz.

suggest us whether I need to change any heap, stack and data address or I should untick any exception.

0 项奖励
回复
5,584 次查看
alexander_yakov
NXP Employee
NXP Employee

The root cause of this problem is in some sensitive registers corrupted during initial device initialization before entering this __start subroutine.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
5,580 次查看
hwrobel
NXP Employee
NXP Employee

Check in Mixed mode after Download first if your memory content is ok.

If you just look at the source view, you may not see the full picture.