Single Bit Error - ECC bits Definition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Single Bit Error - ECC bits Definition

3,072件の閲覧回数
thomaslaughlin
Contributor I

re: MCP8347E

When a single bit error occurs, what value do we expect to see in ECE bit filed for register CAPTURE_ECC:

             Compilation (MOD2) of all the bits selected for a specific ECC bit?

             The value from the table depicting a specific bit?

Thanks,

-Tom

3 返答(返信)

2,695件の閲覧回数
Bulat
NXP Employee
NXP Employee

ECE field indicates captured ECC bits on the bus when an ECC error is detected. Nothing is compilated or depicted.

Regards,

Bulat

0 件の賞賛
返信

2,695件の閲覧回数
thomaslaughlin
Contributor I

Hi Bulat,

I’m sorry, with your reply, I don’t have a greater understanding of the ECC bits in the register.

Let me ask in a different way:

If while in execution a single bit error is detected, how do I use the ECC bits to diagnose the source?

Thanks,

-Tom

0 件の賞賛
返信

2,695件の閲覧回数
Bulat
NXP Employee
NXP Employee

ECC bits are not normally intended to be used by the user, or in other words ECE field value itself is useless for any kind of diagnose. As you might know, the DDR controller automatically corrects single-bit errors. The best what can user do in case of a single-bit error, is to write back correct value to the address indicated by the CAPTURE_ADDRESS register.

Regards,

Bulat