Should QUICC Engine in MPC8569E use soft uart or ordinary uart?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Should QUICC Engine in MPC8569E use soft uart or ordinary uart?

跳至解决方案
1,272 次查看
yunyuaner
Contributor I

I'm trying to use ucc uart provided by QUICC Engine in MPC8569E, and I've checked the ucc_uart.c in linux kernel. However, I can't find the corresponding "fsl_qe_ucode_uart_%u_%u%u.bin" file in nxp's website. Seems the ucode is required only if in soft uart mode. Does anybody know if MPC8569E should use soft uart or ordinary uart? If soft uart should be used, where can I get the ucode or is there any script that can be used to generate it?

Thanks

Jia

0 项奖励
回复
1 解答
1,210 次查看
alexander_yakov
NXP Employee
NXP Employee

UCC UART is not soft UART, this is UART mode of UCC controller. UCC controller is hardware controller, this controller is a part of QE ("Quicc Engine") communication co-processor. This QE is actually another processor which its own software (microcode). This microcode can be either pre-programmed on factory to onchip ROM or loaded to internal RAM every time the device is powered. The MPC8569 processor does not have onchip ROM for QE microcode, to this microcode must be loaded to onchip RAM at device power on.

QE microcode binary image is distributed as a part of our Linux BSP for MPC8569-based "MDS" board.

Direct link to MPC85xx BSPs download page:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,211 次查看
alexander_yakov
NXP Employee
NXP Employee

UCC UART is not soft UART, this is UART mode of UCC controller. UCC controller is hardware controller, this controller is a part of QE ("Quicc Engine") communication co-processor. This QE is actually another processor which its own software (microcode). This microcode can be either pre-programmed on factory to onchip ROM or loaded to internal RAM every time the device is powered. The MPC8569 processor does not have onchip ROM for QE microcode, to this microcode must be loaded to onchip RAM at device power on.

QE microcode binary image is distributed as a part of our Linux BSP for MPC8569-based "MDS" board.

Direct link to MPC85xx BSPs download page:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

0 项奖励
回复