SRIO Driver for MPC8641d

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRIO Driver for MPC8641d

1,004 Views
shrikantkumar
Contributor I

I am trying to develop SRIO driver for MPC8641d.

Currently i am able to send and receive doorbell messages correctly

So it means there is no issue with the backplane connectivity

But sending & Receiving of Data is not working. What could be the possible reason for this?

Tags (1)
0 Kudos
Reply
1 Reply

878 Views
Pavel
NXP Employee
NXP Employee

Look at attached files. This attachment contains SRIO for Linux BSP for the MPC8641:

https://www.nxp.com/webapp/Download?colCode=CWF-MPC8641&appType=license

 

See description in the .html file and driver codes.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply