Replacement for MPC880CVR133

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Replacement for MPC880CVR133

2,058 次查看
mohammedashif_s
Contributor II

Hi,

PowerQUICC Processors‌QorIQ Processing PlatformsColdFire/68K Microcontrollers and Processors‌MPC5xxxnxpftftechforumNXP Designs

   I'm looking for direct replacement or any suitable alternate for MPC880CVR133. This IC has gone obsolete.

I found MPC8306SCVMABDCA with similar specs but any suggestions?

Thanks,

Ashif

3 回复数

1,958 次查看
bpe
NXP Employee
NXP Employee

There are no drop-in replecements for MPC880. Besides MPC830x,
potential candidates can be P1010, LS1012, LS1021, LS1028, depending

on the requirements of the application.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,958 次查看
mohammedashif_s
Contributor II

Hi, 

   MPC880 seems to be low end processor. I'm looking for possibilities to replace with a micro controller with similar specifications. Same architecture would be helpful if available.

Main requirements:

32 bit single core with 32 Data and Addr lines

113Mhz core freq.

Fast ethernet: 10/100Mbps via MII/RMII

Memory: DRAM or above

Any recommendations?

Thanks,

Ashif

0 项奖励
回复

1,958 次查看
bpe
NXP Employee
NXP Employee

The criteria you specified are matched by multiple products in several
families. Your can use NXP online Product selector to see the choice.


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复