Regarding MPC8640D Processor based board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding MPC8640D Processor based board

1,514 次查看
nagajyothi
Contributor I

Hi all,

We are working on a project CPCI Based SBC Board using MPC8640D processor.

We are working with our developed board since last two months successfully.

Recently we got a problem with our board while using. We are facing the

problem with Failed to reset the target (MPC8640d Core.

Again we are in initial stage problem. We are suspecting the power and

clock signals, everything is fine. And hardware reset of the board is also

fine.

Here, I attached log file. Please look at this once.

The following error is getting in log file.

CCS: 0000 : ccs_reset_to_debug

CCS: : serverh = 0

CCS: : cc = 0

CCS: : ccs_reset_to_debug; ccs_error = 39

CCS: : Error message:

MPC8641 Core: Core not responding

Can you give me some guidance in interpreting this error ?

Thanks and Regards,

Jyothi

0 项奖励
回复
1 回复

1,415 次查看
alexander_yakov
NXP Employee
NXP Employee

Please verify processor power supplies, configuration pins and clock input.

In case if you have more than one board - please check if the problem appears on another board.

0 项奖励
回复