Re: Linux Kernel Debugging Using USBTAP and Codewarrior Development studio( Classic IDE)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: Linux Kernel Debugging Using USBTAP and Codewarrior Development studio( Classic IDE)

1,922件の閲覧回数
ashishkhetan
Contributor II

Hi,

I was trying to load vxworks bootloader elf format file using file->open, and it always failing displaying two files added one is dummy.c and another one readme. when using same method i tried to open linux kernel image it successfully loaded the file and shows up the source. Have anyone used codewarrior to debug vxworks? Any pointer/text will be really helpful.

0 件の賞賛
返信
1 返信

1,762件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

I've reviewed our knowledgebase and I do not see any previous experience debugging VxWorks using CodeWarrior devepopment tools.

0 件の賞賛
返信