Question about switching task on mpc8306

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about switching task on mpc8306

4,007 Views
maojiu
Contributor I

I am porting some embedded system to mpc8306 and  switch my tasks in the function handling timer interrupt. I  know that the basic concept of task switching is to save the values of all the registers working for current task  and reload the values of the registers for another task. Since all the register should be saved for current task to the task's stack,  I think the meaning of  the first several statements in the timer interrupt function should be like "lwz  r1,(address of current task stack) ".  Thus, my question is: how can I save the value of "r1" since it is written before I get the stack address ?

0 Kudos
Reply
6 Replies

3,764 Views
lunminliang
NXP Employee
NXP Employee

Maybe you can share more pseudo code to analyze for the specific question...

0 Kudos
Reply

3,764 Views
maojiu
Contributor I

My assembly code in timer interrupt handler is like the following:

vTimerInteruptHandler:

  mtspr 272,r1

  lwz  r1, (currentStack)------------get the address of current task's stack

   stw r4, XR4(r1) --------------save r4 to the stack

   mflr r4,

   stw  r4, XLR(r1)--------------save lr to the stack

    lis     r4,     vPortISR@h

    ori     r4, r4, vPortISR@l

    mtlr    r4

    blr

  rfi

vPortISR:

  lwz r4, XLR(r1)

  mtlr r4

  lwz r4, XR4(r1)

  portSAVE_CONTEXT

   # call the c interrupt handler

    lis     r4,     vPortTickIntHandler@h--------------------vPortTickHandler is to switch task, which makes "currentStack" point to the next task's stack

    ori     r4, r4, vPortTickIntHandler@l

    mtlr    r4

    blrl

  portRESTORE_CONTEXT

   rfi

.end

.macro portSAVE_CONTEXT

  stw     r0,  XR0(r1)

  stw     r2,  XR2(r1)                       

  stw     r3,  XR3(r1)

  stw     r4,  XR4(r1)

  stw     r5,  XR5(r1)

  stw     r6,  XR6(r1)

  stw     r7,  XR7(r1)

  stw     r8,  XR8(r1)

  stw     r9,  XR9(r1)

  stw     r10, XR10(r1)

  stw     r11, XR11(r1)

  stw     r12, XR12(r1)

  stw     r13, XR13(r1)

  stw     r14, XR14(r1)

  stw     r15, XR15(r1)

  stw     r16, XR16(r1)

  stw     r17, XR17(r1)

  stw     r18, XR18(r1)

  stw     r19, XR19(r1)

  stw     r20, XR20(r1)

  stw     r21, XR21(r1)

  stw     r22, XR22(r1)

  stw     r23, XR23(r1)

  stw     r24, XR24(r1)

  stw     r25, XR25(r1)

  stw     r26, XR26(r1)

  stw     r27, XR27(r1)

  stw     r28, XR28(r1)

  stw     r29, XR29(r1)

  stw     r30, XR30(r1)

  stw     r31, XR31(r1)

  mfmsr   r0

  stw     r0,  XMSR(r1)

  mfspr   r0,  SRR0

  stw     r0,  XSRR0(r1)

  mfspr   r0,  SRR1

  stw     r0,  XSRR1(r1)

  mflr    r0

  stw     r0,  XLR(r1)

  mfcr    r0

  stw     r0,  XCR(r1)

  mfctr   r0

  stw     r0,  XCTR(r1)

  mfxer   r0

  stw     r0,  XXER(r1)

  mfmsr   r0

  stw     r0,  XMSR(r1)

  mfspr  r0,272

  stw    r0,XR1(r1)

  .endm

  .macro portRESTORE_CONTEXT

  lwz  r1, (currentStack)

  lwz     r0,  XSRR0(r1)

  mtspr   SRR0,r0

  lwz     r0,  XSRR1(r1)

  mtspr   SRR1,r0

  lwz     r0,  XLR(r1)

  mtlr    r0

  lwz     r0,  XCR(r1)

  mtcrf   0xff,r0

  lwz     r0,  XCTR(r1)

  mtctr   r0

  lwz     r0,  XXER(r1)

  mtxer   r0

  lwz     r0,  XR0(r1)

  lwz     r2,  XR2(r1)

  lwz     r3,  XR3(r1)

  lwz     r4,  XR4(r1)

  lwz     r5,  XR5(r1)

  lwz     r6,  XR6(r1)

  lwz     r7,  XR7(r1)

  lwz     r8,  XR8(r1)

  lwz     r9,  XR9(r1)

  lwz     r10, XR10(r1)

  lwz     r11, XR11(r1)

  lwz     r12, XR12(r1)

  lwz     r13, XR13(r1)

  lwz     r14, XR14(r1)

  lwz     r15, XR15(r1)

  lwz     r16, XR16(r1)

  lwz     r17, XR17(r1)

  lwz     r18, XR18(r1)

  lwz     r19, XR19(r1)

  lwz     r20, XR20(r1)

  lwz     r21, XR21(r1)

  lwz     r22, XR22(r1)

  lwz     r23, XR23(r1)

  lwz     r24, XR24(r1)

  lwz     r25, XR25(r1)

  lwz     r26, XR26(r1)

  lwz     r27, XR27(r1)

  lwz     r28, XR28(r1)

  lwz     r29, XR29(r1)

  lwz     r30, XR30(r1)

  lwz     r31, XR31(r1)

  lwz     r1,     0(r1)

.endm

0 Kudos
Reply

3,764 Views
scottwood
NXP Employee
NXP Employee

Why "lwz r1, 0(r1)" rather than "lwz r1, XR1(r1)"?

0 Kudos
Reply

3,764 Views
maojiu
Contributor I

Thank you for your help and sorry for not making my code clear. XR1 equals to 0 in my context. I just want to make sure if I saved all the resgisters that I should.

0 Kudos
Reply

3,764 Views
scottwood
NXP Employee
NXP Employee

This question seems to be more about state saving for exception entry rather than switching tasks, but the usual approach is to use a SPRG as temporary storage.

0 Kudos
Reply

3,764 Views
maojiu
Contributor I

I have used SPRG0 according to your advice and the situation looks like better, but it is still not working. I saved the following registers for state saving in timer interrupt handler:

r0 to r31, srr0,srr1, msr,lr, ctr, cr, xer.

I wonder if there are any other registers I should save ?

0 Kudos
Reply