Question about MPC8280's SDRAM machine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about MPC8280's SDRAM machine

ソリューションへジャンプ
2,521件の閲覧回数
春新张
Contributor I

Hi All,

Here is a project use MPC8280. I use SDRAM machine connect SDRAM(32M16A2).The SDRAM have 4 internal banks, 13 rows, and 10 columns.

I  reference 《MPC8280RM Rev. 1, 12/2005》,11.4.5.2 SDRAM Address Multiplexing (SDAM and BSMA),but still have same

questions.

The reference book have examples,but all the examples are about SDRAM devices that have 4 internal banks, 12 rows, and 9 columns.

I copy the tables below.

My question is:

what is the meaning "-",is that I cann't use the pin?

for example I set SDMR[SDAM] = 100; Can I use A[14–15] for bank select pins?

未命名.bmp

0 件の賞賛
返信
1 解決策
2,353件の閲覧回数
Bulat
NXP Employee
NXP Employee

"-" in the table means no address muxing for SDRAM's address signals during ACTIVATE command. This does not relate to the bank select signals, only to address ones. Muxing of bank select signals is defined by the xSDRAM[BSMA] field. The answer to your question: yes, you can use A[14–15] as bank selects if xSDRAM[BSMA] is properly set (BSMA=0b001).

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,353件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Sorry, I made a mistake here. The Table 11-20 is for address multiplexing of row address, here "-" means for that "SDAM" configuration the physical address kine will not ouput mux address. A[14-15] can be used for bank select if configured by BSMA.

0 件の賞賛
返信
2,353件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Just to add to the Bulat' response - this setup "4 internal banks, 13 rows, and 10 columns" is described as Example 1 in application note AN2165 "MPC8260 SDRAM Support".

http://cache.freescale.com/files/32bit/doc/app_note/AN2165.pdf

0 件の賞賛
返信
2,354件の閲覧回数
Bulat
NXP Employee
NXP Employee

"-" in the table means no address muxing for SDRAM's address signals during ACTIVATE command. This does not relate to the bank select signals, only to address ones. Muxing of bank select signals is defined by the xSDRAM[BSMA] field. The answer to your question: yes, you can use A[14–15] as bank selects if xSDRAM[BSMA] is properly set (BSMA=0b001).

0 件の賞賛
返信
2,353件の閲覧回数
lunminliang
NXP Employee
NXP Employee

I am afraid no, if setting SDAM to be "100", you can not use A14 and A15.

0 件の賞賛
返信