Programming the MPC8360

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming the MPC8360

2,555件の閲覧回数
hvdmerwe
Contributor II

Good Day,

We are migrating from the MPC8260 Processor to the MPC8360. On the MPC8260 we pull the RSTCONF_ pin low to place the the Processor in defualt config to allow configuration. 

Is there in Pin/ signal that needs to be asserted/negated to allow programming of the MPC8360 via the COP/JTAG signals? Is there a guide available that explains the physical programming or flashing of the MPC8360 processor cia the COP/JTAG signals?

Kind Regards

タグ(4)
0 件の賞賛
返信
3 返答(返信)

2,474件の閲覧回数
r8070z
NXP Employee
NXP Employee

The MPC8360 CFG_RESET_SOURCE[0:2] pins is analog of the MPC8260 RSTCONF pin. These pins select reset configuration word source. Correct operation of the JTAG interface requires configuration of a group of system control pins as described and demonstrated in the Design Checklist document
https://www.nxp.com/docs/en/application-note/AN3097.pdf
See section " JTAG and Debug ". The JTAG test interface (based on IEEE 1149.1) provides a means for boundary-scan testing of the core and the attached system logic. The hardware debug function accesses the JTAG test port, providing a

means for executing test routines and facilitating chip and software debugging. As guide see for example Hardware Debugging Using the CodeWarrior™ IDE document

https://www.nxp.com/docs/en/application-note/AN3830.pdf

2,474件の閲覧回数
hvdmerwe
Contributor II
Thank you for the reply,

How does the PowerQuicc know that you want to program it with something new.

From what I can gather, the CFG_RESET_SOURCE[0:2] just tells the PowerQuicc where to look for the reset configuration word.

Is there a guide to explain how to program the Powerquicc, or how to program a local bus SRAM/Flash via the Powerquicc? I think that is what I am struggling most with at the time.
0 件の賞賛
返信

2,474件の閲覧回数
r8070z
NXP Employee
NXP Employee

Yes as I wrote the MPC8360 CFG_RESET_SOURCE[0:2] are like the MPC8260 RSTCONF. 
There are guide for the tools which can program a local bus SRAM/Flash via the Powerquicc only.  These tools use the JTAG/COP interface.  Special COP protocol used to Displaying Memory and Registers like in the AN3830 it also permit download code and program Flash connected to the MPC8360. So the CodeWarrior™ includes FLASH programmer. 

0 件の賞賛
返信