Processor recommendations for 3U VPX Card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor recommendations for 3U VPX Card

2,561件の閲覧回数
adosa3
Contributor I

Hi. I need to make a custom  3U VPX card PCB. The requirements are:

- support for 1000base-kx (backplane Ethernet); only 1G protocol supported by most 3U VPX Ethernet Switches  

- Interfaces: SPI, UART, I2C

This is not a heavy processing unit, so 1GB DDR is enough. Which processors do you recommend? 

I found the 1023a/1043a as being the lowest pin count/lowest complexity. Are there any other ones that I might have missed? 

Thank you. 

0 件の賞賛
返信
2 返答(返信)

2,556件の閲覧回数
ufedor
NXP Employee
NXP Employee

2,548件の閲覧回数
adosa3
Contributor I

Brilliant. Thank you!

0 件の賞賛
返信