Processor recommendations for 3U VPX Card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Processor recommendations for 3U VPX Card

2,571 次查看
adosa3
Contributor I

Hi. I need to make a custom  3U VPX card PCB. The requirements are:

- support for 1000base-kx (backplane Ethernet); only 1G protocol supported by most 3U VPX Ethernet Switches  

- Interfaces: SPI, UART, I2C

This is not a heavy processing unit, so 1GB DDR is enough. Which processors do you recommend? 

I found the 1023a/1043a as being the lowest pin count/lowest complexity. Are there any other ones that I might have missed? 

Thank you. 

0 项奖励
回复
2 回复数

2,566 次查看
ufedor
NXP Employee
NXP Employee

2,558 次查看
adosa3
Contributor I

Brilliant. Thank you!

0 项奖励
回复