Problem with Codewarrior tap on ubuntu 14.04 LTS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with Codewarrior tap on ubuntu 14.04 LTS

1,361 次查看
badrinatht
Contributor I

I have working with codewarrior power architecture 8.8 IDE on windows 7 PC. On this PC my codewarrior tap is working nice. But on linux system, am getting error  "USB open failure" . I have installed Ubuntu 14.04 on new PC and codewarrior power architecture 8.8 linux host on it . I have attached ccs log file to this message.

Original Attachment has been moved to: ccs_log.txt.zip

0 项奖励
回复
1 回复

1,097 次查看
Pavel
NXP Employee
NXP Employee

If CodeWarrior 8.8 is used under Windows 7, CodeWarrior 8.6 patch is used for CodeWarrior TAP driver installation.

There is no similar patch for Linux.

Look at attached file. This file contains recommendations for CodeWarrior TAP driver installing under Linux.

Test your board using these recommendations.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复