Problem setting SRDS registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem setting SRDS registers

1,775 Views
carlessilva
Contributor I

I'm trying to use the SATA devices in the MPC8379 evalutaion board. I'm having problems while updating the SRDS registers so it's programmed to use SATA interface.

I'm trying to set the following values:

SRDSCR0: 0x1100CC30

SRDSCR1: 0x00000040

SRDSCR2: 0x00001414

SRDSCR3: 0x15150528

SRDSCR4: 0x40000808

However this registers are always with the reset values. Should I do something else before being able to edit those registers?

0 Kudos
Reply
2 Replies

1,670 Views
Pavel
NXP Employee
NXP Employee

Look at the Section 19.4 of the MPC8379 Reference Manual. This Section contains command sequence for SerDes and PHY initialization and Reset.

Test your board using this command sequence.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,670 Views
carlessilva
Contributor I

Pavel,

thanks for your response. This is exactly the sequence I'm following but still SATA device's are not working. I'm following the code I'm using in the MPC8315, adding the initialization of the SerDes PHY.

Any clue in what the problem may be?

0 Kudos
Reply