Performance of PowerQUICC MPC8548

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Performance of PowerQUICC MPC8548

1,438件の閲覧回数
oscarchinellato
Contributor I

Dear all,

I would like to obtain information about the performance (MIPS, FLOPS, etc.) of the Freescale PowerPC PowerQUICCTM III MPC8548 processor.

Could you help me by pointing out to me where to find any?

Many thanks in advance,
Oscar Chinellato

0 件の賞賛
返信
1 返信

1,217件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

On the MPC8548 page of the NXP site they say: “Embedded e500 core, scaling up to 1.5 GHz … 3065 MIPS at 1333 MHz (estimated Dhrystone 2.1)”. The Coremark benchmark gave 3.6 CMark/MHz.

The peak FP performance is 2 single precision operations, or one double precision FP operation per core clock cycle. For instruction execution timing you may see Chapter 4 of the E500 core reference manual (E500CORERM).

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信