P2040/2041 Linux kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P2040/2041 Linux kernel

ソリューションへジャンプ
2,224件の閲覧回数
sergiomarques
Contributor II
I need to upgrade the 4.1.35 kernel I am using in a project whith a P2040. Must be a version kernel higher then 4.2.1. Where can I get such kernel?
0 件の賞賛
返信
1 解決策
2,215件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could use the latest Yocto 3.1 SDK release from NXP, please refer to "https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=dunfell"

Yocto 3.1 release integrates Linux Kernel 5.4, it supports P2041RDB platform.

In addition, you also could use Yocto 2.5/2.6 release, it integrates Linux Kernel 4.9 and 4.14, please refer to the following link.

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=thud

元の投稿で解決策を見る

1 返信
2,216件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could use the latest Yocto 3.1 SDK release from NXP, please refer to "https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=dunfell"

Yocto 3.1 release integrates Linux Kernel 5.4, it supports P2041RDB platform.

In addition, you also could use Yocto 2.5/2.6 release, it integrates Linux Kernel 4.9 and 4.14, please refer to the following link.

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=thud