P2040/2041 Linux kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2040/2041 Linux kernel

Jump to solution
2,249 Views
sergiomarques
Contributor II
I need to upgrade the 4.1.35 kernel I am using in a project whith a P2040. Must be a version kernel higher then 4.2.1. Where can I get such kernel?
0 Kudos
Reply
1 Solution
2,240 Views
yipingwang
NXP TechSupport
NXP TechSupport

You could use the latest Yocto 3.1 SDK release from NXP, please refer to "https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=dunfell"

Yocto 3.1 release integrates Linux Kernel 5.4, it supports P2041RDB platform.

In addition, you also could use Yocto 2.5/2.6 release, it integrates Linux Kernel 4.9 and 4.14, please refer to the following link.

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=thud

View solution in original post

1 Reply
2,241 Views
yipingwang
NXP TechSupport
NXP TechSupport

You could use the latest Yocto 3.1 SDK release from NXP, please refer to "https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=dunfell"

Yocto 3.1 release integrates Linux Kernel 5.4, it supports P2041RDB platform.

In addition, you also could use Yocto 2.5/2.6 release, it integrates Linux Kernel 4.9 and 4.14, please refer to the following link.

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/tree/readme?h=thud