P1021rdb not able to ping using eTSEC2 in SGMII mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

P1021rdb not able to ping using eTSEC2 in SGMII mode

跳至解决方案
2,942 次查看
solomon
Contributor II

Hi,

I'm having a problem not being able to ping to an ipaddress. I'm wokring on P1021rdb PowerQUICC based processor, configured eTSEC2 in SGMII mode. The link shows being "Link - Up" but unable to ping

I'm only using ethernet 1 (eTSEC2 in SGMII mode)

Please find all the info regarding the board bring up, uboot output, dts,
bootUp file and Application which configures the ethernet is attached
Please go through the files.


DTS:

==========p1021rdb-pc.dtsi========

&soc {

mdio@25000 {
tbi1:tbi-phy@1f {
reg = <0x1f>;
device_type = "tbi-phy";
};
};

enet1: ethernet@b1000 {
// fixed-link =<31 1 1000 0 0>;
//phy-handle = <&phy0>;
phy-handle = <&tbi1>;
tbi-handle = <&tbi1>;
phy-connection-type = "sgmii";
};


};

=========p1021si-pre.dtsi=========

aliases {
serial0 = &serial0;
serial1 = &serial1;
// ethernet0 = &enet0;
ethernet1 = &enet1;
// ethernet2 = &enet2;
// pci0 = &pci0;
// pci1 = &pci1;
};


========p1021si-post.dtsi==========

enet1: enet1_grp2: ethernet@b1000 {
// ptimer-handle = <&ptp_timer>;
fsl,pmc-handle = <&etsec2_clk>;
};


global-utilities@e0000 {
compatible = "fsl,p1021-guts";
reg = <0xe0000 0x1000>;
fsl,has-rstcr;
};


=========pq3-etsec2-1.dtsi=======
mdio@25000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,gianfar-tbi"; //changed from etsec2-tbi to gianfar-tbi since tbipa = 0x030
reg = <0x25000 0x1000 0xb1030 0x4>;
};

ethernet@b1000 {
#address-cells = <1>;
#size-cells = <1>;
device_type = "network";
model = "eTSEC";
compatible = "fsl,etsec2";
fsl,num_rx_queues = <0x8>;
fsl,num_tx_queues = <0x8>;
fsl,magic-packet;
local-mac-address = [ 00 11 22 33 44 77 ];
ranges;

queue-group@b1000 {
#address-cells = <1>;
#size-cells = <1>;
reg = <0xb1000 0x1000>;
interrupts = <35 2 0 0 36 2 0 0 40 2 0 0>;
};
};

==========pq3-etsec2-grp2-1.dtsi============
&enet1_grp2 {
queue-group@b5000 {
#address-cells = <1>;
#size-cells = <1>;
reg = <0xb5000 0x1000>;
interrupts = <51 2 0 0 52 2 0 0 67 2 0 0>;
};
};


======UBOOT========
==>print
eth1addr=00:11:22:02:01:01
eth2addr=00:11:22:02:01:01
ethact=eTSEC2
ethaddr=00:11:22:33:44:55
ethprime=eTSEC2
ipaddr=192.168.30.176

=> mdio list
FSL_MDIO:
0 - Generic PHY <--> eTSEC2
15 - TI DP83867 <--> eTSEC3
17 - Generic PHY <--> eTSEC1

 

==============
After board bringUp, we created an application which configures the ethernet,
we are using ELECTRICAL SFP (Finisar).
Application successfully configures the ethernet and the Link is Up,
but not able to use PING

Attached the BootUp file and Application Output File. Please check the files
===============================

=========ethtool=========
root@p1021rdb:~# ethtool eth0
Settings for eth0:
Supported ports: [ MII ]
Supported link modes: 1000baseT/Full
Supported pause frame use: Symmetric Receive-only
Supports auto-negotiation: Yes
Advertised link modes: 1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Speed: 1000Mb/s
Duplex: Full
Port: MII
PHYAD: 31
Transceiver: external
Auto-negotiation: on
Supports Wake-on: g
Wake-on: d
Current message level: 0x0000003f (63)
drv probe link timer ifdown ifup
Link detected: yes

root@p1021rdb:~# ethtool -a eth0
Pa Ker: gfar_gpauseparam epause->autoneg: 0 epause->rx_pause: 0 epause->tx_pause: 0
use parameters for eth0:
Autonegotiate: off
RX: off
TX: off


============PING=================

root@p1021rdb:~# ping 192.168.30.123
PIN Ker: gfar_start_xmit
G 192.168.30.123 (192.168.30.123) 56(84) bytes of data.
Ker: gfar_start_xmit
Ker: gfar_start_xmit
Ker: gfar_start_xmit
From 192.168.30.51 icmp_seq=1 Dest Ker: gfar_start_xmit
ination Host Unreachable
From 192.168.30.51 icmp_seq=2 Destination Host Unreachable
From 192.168.30.51 icmp_seq=3 Destination Host Unreachable
Ker: gfar_start_xmit
Ker: gfar_start_xmit
From 192.168.30.51 icmp_seq=4 Desti Ker: gfar_start_xmit
nation Host Unreachable
From 192.168.30.51 icmp_seq=5 Destination Host Unreachable
From 192.168.30.51 icmp_seq=6 Destination Host Unreachable
^C
--- 192.168.30.123 ping statistics ---
7 packets transmitted, 0 received, +6 errors, 100% packet loss, time 6000ms
pipe 3
root@p1021rdb:~# Ker: gfar_start_xmit

 

========
Awaiting for response
Thank you

 

0 项奖励
回复
1 解答
2,871 次查看
solomon
Contributor II

Found the solution for the error.

I was going through the Gianfar.c and in the gfar_start() function I've observed that the below two lines of code which enables the queues were commented.

gfar_write(&regs->rqueue, priv->rqueue);
gfar_write(&regs->tqueue, priv->tqueue);

i don't remember why it was commented out, but thank you for the support given

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,932 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please define enet1 similar as the following.

enet1: ethernet@b1000 {
phy-handle = <&phy0>;
tbi-handle = <&tbi1>;
phy-connection-type = "sgmii";

}

 

mdio@24000 {

phy0: ethernet-phy@0 {

interrupt-parent = <&mpic>;

interrupts =<3  1 0 0>;

 reg = <0x0>;

  };

...

 

0 项奖励
回复
2,872 次查看
solomon
Contributor II

Found the solution for the error.

I was going through the Gianfar.c and in the gfar_start() function I've observed that the below two lines of code which enables the queues were commented.

gfar_write(&regs->rqueue, priv->rqueue);
gfar_write(&regs->tqueue, priv->tqueue);

i don't remember why it was commented out, but thank you for the support given

0 项奖励
回复
2,897 次查看
solomon
Contributor II

Sorry i did not provide complete imformation

We are using Finisar (electrical) phy, where it is being configured via I2C.
For data transfer we are using SerDes in SGMII mode and eTSEC2 with internal TBI PHY is used.

0 项奖励
回复
2,877 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello solomon,

 

You need to contact the PHY manufacturer for driver availability.

Please refer to https://elixir.bootlin.com/linux/latest/source/drivers/net/phy/mdio-i2c.c

You need to replace phy_read()/phy_write in PHY device driver with i2c read/write functions.

0 项奖励
回复