Orcad schematic on MPC8313

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Orcad schematic on MPC8313

10,094 Views
mii
Contributor I
Hi,
I am looking for the orcad schematic on MPC8313.
There is nothing in the freescale website.
If somebody has it, can you send it to me, please ?
Thanks in avance.
Regards
Mii
0 Kudos
Reply
5 Replies

4,000 Views
armdev
Contributor I
开发板,深圳诚拓科技,专业高端POWERPC、ARM、MIPS开发板、仿真器、ICE、评估板、成熟技术方案提供商
powerpc开发板,powerpc仿真器powerpc开发板,powerpc仿真器,深圳诚拓科技 提供 powerpc开发板,powerpc仿真器,整套解决方案
powerpc仿真器USB TAP,支持CodeWarrior软件POWERPC、MPC、PPC USB TAP仿真器.调试器( CodeWarrior 调试软件),freescale powerpc USBTAP仿真器,支持CodeWarrior软件,USB TAP调试器,ICE,最好的POWERPC开发调试工具USB TAP,支持CodeWarrior软件单步跟踪,烧写FLASH
MPC8313开发板,MPC8313E开发板,MPC8313E-RDB MPC8313开发板.MPC8313评估板,深圳诚拓提供MPC8313 OEM,ODM服务,MPC8313设备,MPC8313产品开发,成熟的MPC8313设计方案
MPC8315开发板,MPC8315E开发板,MPC8315E-RDB MPC8315开发板,MPC8315评估板,MPC8315产品开发,成熟的MPC8315 设计,提供MPC8315 OEM,ODM服务
MPC8349开发板,MPC8349E开发板,MPC8349E-RDB MPC8349开发板,MPC8349评估板,成熟的MPC8349 设计,MPC8349产品开发,提供MPC8349 OEM,ODM服务
MPC8379开发板,MPC8379E开发板,MPC8379E-RDB MPC8379开发板,MPC8379评估板,MPC8379E开发板,专注MPC8379,MPC8379E设备开发,MPC8379,MPC8379E产品开发,专业MPC8379,MPC8379E 设计,成熟的MPC8379,MPC8379E OEM,ODM技术服务
MPC8540开发板,MPC8540开发板,MPC8541,MPC8541E,MPC8555,MPC8555E,MPC8560开发板,MPC8560评估板,MPC8540评估板,MPC8540开发板,专注MPC8540设备开发,MPC8540 OEM 产品,专业MPC8540设计,成熟的MPC8540 OEM,ODM技术服务
MPC8541开发板,MPC8541E开发板,MPC8540,MPC8541开发板,MPC8541E开发板,MPC8555,MPC8555E,MPC8560开发板,MPC8560评估板,MPC8541评估板,MPC8541开发板,MPC8541E开发板,专注MPC8541,MPC8541E设备开发,专业MPC8540,MPC8541E设计,MPC8541,MPC8541E产品开发,成熟的MPC8541,MPC8541E,ODM技术服务
MPC8555开发板,MPC8555E开发板,MPC8540,MPC8541,MPC8541E,MPC8555开发板,MPC8555E开发板,MPC8560开发板,MPC8560评估板,MPC8555评估板,MPC8555开发板,MPC8555E开发板,专业MPC8555,MPC8555E设计,专注MPC8555,MPC8555E设备开发,MPC8555,MPC8555E产品开发,成熟的MPC8555,MPC8555E,ODM技术服务
MPC8560开发板,MPC8560评估板,MPC8540,MPC8541,MPC8541E,MPC8555,MPC8555E,MPC8560开发板,MPC8560评估板,MPC8560评估板,MPC8560开发板,成熟的MPC8560,OEM,ODM技术服务,专业MPC8560设计,专注MPC8560芯片开发,MPC85600产品开发
MPC8270开发板,MPC8270开发板,MPC8270评估板,MPC8270评估板
MPC8280开发板,MPC8280开发板,MPC8280评估板,MPC8280评估板
MPC8271开发板,MPC8272开发板,MPC8271开发板,MPC8272评估板,MPC8271评估板,MPC8272开发板
MPC8247开发板,MPC8248开发板,MPC8247开发板,MPC8248评估板,MPC8247评估板,MPC8248开发板
MPC5200开发板,MPC5200B开发板,MPC5200开发板,MPC5200B评估板,MPC5200评估板,MPC5200B开发板
MPC5121开发板,MPC5121E开发板,MPC5123开发板,MPC5123E开发板,MPC5121开发板,MPC5121E开发板,MPC5123,MPC5123E开发板,MPC5125,MPC5125E开发板,评估板,深圳诚拓提供MPC5121E开发服务,MPC5121E产品开发,MPC5121E OEM,ODM技术服务,MPC5121E委托开发
MPC8360开发板,MPC8360E开发板,MPC8358开发板,MPC8358E开发板,MPC8360E开发板,MPC8360开发板,MPC8360评估板,MPC8360E开发板,深圳诚拓提供成熟的MPC8360,MPC8360E OEM,ODM技术服务,专注于MPC8360,MPC8360E设备开发,MPC8360,MPC8360E产品开发,专业MPC8360,MPC8360E 设计
MPC8568E-MDS开发板,MPC8568E-MDS开发板,MPC8568E-MDS评估板,MPC8568E-MDS评估板,适合于MPC8568E产品开发,MPC8568E功能测试,MPC8568E性能评估
MPC8548开发板,MPC8548E开发板,MPC8548E,MPC8548开发板,MPC8548评估板,MPC8548E开发板,专业MPC8548,MPC8548E 设计,专注MPC8548,MPC8548E设备开发,MPC8548,MPC8548E产品开发,成熟的MPC8548,MPC8548E OEM,ODM技术服务
MPC8377EWLAN开发板,802.11N网关,无线AP接入产品开发MPC8377EWLAN开发板,MPC8377EWLAN评估板(CPU MPC8377 MPC8377E),最专业的MPC8377开发平台,MPC8377EWLAN评估板,完善的802.11N产品.MPC8377评估板,MPC8377E开发板,专注MPC8377,MPC8377E设备开发,MPC8377,MPC8377E产品开发,专业MPC8377,MPC8377E 设计,成熟的MPC8377,MPC8377E平台
IXP430 IXP435 OEM ODM模块IXP430 IXP431 IXP432 IXP433 IXP434 IXP435 OEM ODM模块,最适合你的IXP430 IXP435 OEM ODM模块,兼容IXP430、IXP431、IXP432、IXP433、IXP435等CPU。ixp430 ixp435 OEM模块CPU为IXP435 667M主频,128M DDR2 内存,16M nor flash,2个USB高速HOST接口(480M bps),2个100M 网口,2个MINIPCI.IXP435 IXP430 OEM模块适合于无线网桥,soho 网关,vpn 网关,802.11a/b/g wifi AP
IXP430 IXP435 开发板IXP430 IXP431 IXP432 IXP433 IXP434 IXP435 开发板,基于intel ixp43x网络处理器系列的开发板,支持IXP430,IXP431,IXP432,IXP433,IXP434,IXP435.ixp435开发板上焊的cpu为ixp435 667M主频,128M DDR2 内存,16M nor flash,2个100M 网口,2个USB高速接口(480M bps),2个PCI和1个MINIPCI.CTDB-IXP435 是国内功能最全、接口最全的IXP435开发板.
0 Kudos
Reply

4,000 Views
aurelihein
Contributor I
maybe you should check if you are under nda, in this case you should contact your distributor :smileywink:
0 Kudos
Reply

4,000 Views
mii
Contributor I
Thank you for your answer aurelihein, but we have already done this. We have asked our distributor if we could have the Orcad schematic of the MPC8313 and our distributor has asked Freescale, ... and several weeks have passed and we have nothing!!! 
So if somebody has it, it can be very helpful to send it to me.
Thanks in advance.
 
 
 
 
0 Kudos
Reply

4,000 Views
genuap
NXP Employee
NXP Employee
Where are you located? If you let me know who your distributor is we can work through them - unfortunately the information is still sensitive, and under NDA.

 ... Paul

0 Kudos
Reply

4,000 Views
mii
Contributor I
Thank you for your answer Paul.
We are located in France in Paris. And our distributor is ARROW FRANCE.
If you want other information, maybe we can follow this discussion by email. 
 
Regards
0 Kudos
Reply