ODT and additive latency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ODT and additive latency

1,896件の閲覧回数
dallasclow
Contributor II

The ODT_WR_CFG parameter of the CSn_CONFIG register indicates that write latency plus additive latency must be at least 3 to use ODT.  Our application uses an MPC8610 with 64-bit DDR2 w/ECC running at 200 MHz (DDR400).  Nominal CAS Latency is 3 and write latency is 2.  ODT is required.  Can CAS latency of 3, write latency of 2, and additive latency of 1 be used to meet this requirement and utilize ODT?  If so, should the RD_TO_PRE field of the TIMING_CFG_2 register include the additive latency (1 additional clock) or should it just include the t_RTP duration (2 clocks) when additive latency is used?

ラベル(1)
  • DDR

1 返信

1,843件の閲覧回数
Bulat
NXP Employee
NXP Employee

Yes, CAS latency of 3, write latency of 2, and additive latency of 1 is ok to utilize ODT correctly.

RD_TO_PRE should be equal to tRTP,  ADD_LAT should not be added.

Regards,

Bulat