Need suggestions on MPC8377 reset problem.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need suggestions on MPC8377 reset problem.

2,932件の閲覧回数
mvonahnen
Contributor II

I have a failed board (others of the same design are working).  The symptoms are that the MPC8377 comes out of reset, attempts to read the configuration words, but the DDR clocks are never turned on.  After about 6 seconds, the /HRESET line goes low and the process repeats, continually.  When we tried to connect via the emulator, we were unable to load the DDR memory, it was not configured even with Code Warrior.

 

At one time, the board was operational, booting U-Boot and running LINUX.  Any suggestions of what to look at? 

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,025件の閲覧回数
mvonahnen
Contributor II

This problem was resolved.  I test pin was being held at an improper level during device reset, so it was going into a test mode.

0 件の賞賛
返信

2,025件の閲覧回数
gleb_itech
Contributor I
Are you sure? May be it is floating bug...
0 件の賞賛
返信