Hello everyone,
I made a cutom board based on MPC8309twr development board and did not change the hardware design a lot. I move the norflash hip of development board to my board.
So, I thought that the custom board will boot normally, but I only achieved the following message:
U-Boot 2010.06-00077-gd1e0776 (Dec 27 2011 - 19:51:03) MPC83XX
Reset Status:
CPU: e300c3, MPC8309E, Rev: 1.1 at 400 MHz, CSB: 133.333 MHz
Board: Freescale MPC8309_twr
I2C: ready
SPI: ready
DRAM: 128 MiB
FLASH: 32 MiB
Firmware 'Microcode version 0.0.0 for MPC8309 r1.0' for 8309 V1.0
QE: uploading microcode 'Microcode for MPC8309 r1.0'
It stop at this place. Is there any problems in my hardware design or other configuration? Thinks!!!
已解决! 转到解答。
So, if the same flash image works properly on original board, but does not work on your custom board, than the first question - what exactly changed?
Please specify full list of differences.
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
So, if the same flash image works properly on original board, but does not work on your custom board, than the first question - what exactly changed?
Please specify full list of differences.
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------