Mpc8548 Development Environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mpc8548 Development Environment

ソリューションへジャンプ
2,301件の閲覧回数
systick
Contributor II

Hi All, 

I find somewhere a board it has mcp8548 processor its PowerPC arch., now I want to install Linux on this board, I set the U-Boot, I have to install U-Boot to processor, boards has a jtag interface and I have multilink-fx development interface, here is the problem;

How can I set the development environment ? 

タグ(3)
0 件の賞賛
返信
1 解決策
2,059件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers CodeWarrior 8.8 and CodeWarrior TAP for software developing, debugging and Flash programming on the MPC8548 boards:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX

 

Evaluation version of this CodeWarrior provides full functionality during one month.

Use CodeWarrior 8.8 and CodeWarrior TAP for u-boot burning on your board.

 

Lauterbach and TRACE32 also can be used for u-boot burning on the MPC8548 board.

 

See also "Debuggers and Runtime Analysis" on the following page:

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/powerquic...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,060件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers CodeWarrior 8.8 and CodeWarrior TAP for software developing, debugging and Flash programming on the MPC8548 boards:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX

 

Evaluation version of this CodeWarrior provides full functionality during one month.

Use CodeWarrior 8.8 and CodeWarrior TAP for u-boot burning on your board.

 

Lauterbach and TRACE32 also can be used for u-boot burning on the MPC8548 board.

 

See also "Debuggers and Runtime Analysis" on the following page:

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/powerquic...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信