Mpc8548 Development Environment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mpc8548 Development Environment

Jump to solution
2,293 Views
systick
Contributor II

Hi All, 

I find somewhere a board it has mcp8548 processor its PowerPC arch., now I want to install Linux on this board, I set the U-Boot, I have to install U-Boot to processor, boards has a jtag interface and I have multilink-fx development interface, here is the problem;

How can I set the development environment ? 

Tags (3)
0 Kudos
Reply
1 Solution
2,051 Views
Pavel
NXP Employee
NXP Employee

NXP offers CodeWarrior 8.8 and CodeWarrior TAP for software developing, debugging and Flash programming on the MPC8548 boards:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX

 

Evaluation version of this CodeWarrior provides full functionality during one month.

Use CodeWarrior 8.8 and CodeWarrior TAP for u-boot burning on your board.

 

Lauterbach and TRACE32 also can be used for u-boot burning on the MPC8548 board.

 

See also "Debuggers and Runtime Analysis" on the following page:

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/powerquic...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,052 Views
Pavel
NXP Employee
NXP Employee

NXP offers CodeWarrior 8.8 and CodeWarrior TAP for software developing, debugging and Flash programming on the MPC8548 boards:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=CWX-ARCHT-EX

 

Evaluation version of this CodeWarrior provides full functionality during one month.

Use CodeWarrior 8.8 and CodeWarrior TAP for u-boot burning on your board.

 

Lauterbach and TRACE32 also can be used for u-boot burning on the MPC8548 board.

 

See also "Debuggers and Runtime Analysis" on the following page:

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/powerquic...


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply