Maximum 8349 processor frequency for temperature range -40°C ... +105°C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Maximum 8349 processor frequency for temperature range -40°C ... +105°C

跳至解决方案
2,469 次查看
danielefranco
Contributor I

Quote from:

"MPC8349EA PowerQUICC II Pro Integrated Host Processor Hardware Specifications, Rev. 13"

"For temperature range = C, processor frequency is limited to 

with a platform frequency of 266 and up to 533 with a platform

frequency of 333"

It seems that there is a type in the statement above. Which is the maximum processor frequency for the temperature range "C" (i.e. -40...+105)?

With a platform frequency of 333Mhz it is clear to be 533Mhz, but with a platform frequency of 266?

0 项奖励
回复
1 解答
2,394 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Actually for all 834x family (MPC8343, MPC8347 and MPC8349) this note says

For temperature range = C, processor frequency is limited to 400 (PBGA) with a platform frequency of 266 and up to 533 (TBGA) with a platform frequency of 333

Because MPC8349 is TBGA only they change it in way you have read in the MPC8349 hardware specs. For the MPC8343 they correspondingly change it to

“For temperature range = C, processor frequency is limited to 400 with a platform frequency of 266 and up to with a platform frequency of 333”

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,394 次查看
danielefranco
Contributor I

Thanks for the answer.

Do you know if there is a version of the 8349 (or a compatible processor) that works at higher frequency in the extended temperature range?

0 项奖励
回复
2,395 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Actually for all 834x family (MPC8343, MPC8347 and MPC8349) this note says

For temperature range = C, processor frequency is limited to 400 (PBGA) with a platform frequency of 266 and up to 533 (TBGA) with a platform frequency of 333

Because MPC8349 is TBGA only they change it in way you have read in the MPC8349 hardware specs. For the MPC8343 they correspondingly change it to

“For temperature range = C, processor frequency is limited to 400 with a platform frequency of 266 and up to with a platform frequency of 333”

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------