MPC8640 Probe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8640 Probe

2,931件の閲覧回数
arun2
Contributor II

Hi ,

Please help me is there any suitable option for CWH-UTP-PPCC-HE

Regards ,

Arun K Soman

PME

WT Microelectronics

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,292件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

The probe CWH-UTP-PPCC-HE is not available for ordering, but if you have it - it will work with MPC8640

If you need to order a new probe for this device, please other CodeWarrior TAP - partnumbers CWH-CTP-BASE-HE and CWH-CTP-COP-YE (base and JTAG/COP probe tip).

Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,292件の閲覧回数
arun2
Contributor II

Sir ,

I have two queries ,

What will be the tools (Tap and Probe ) which support below parts .

1.     MC8640DTVJ1250HE

2.     MPC8540

Regards ,

Arun K soman

PME

WT Microelectronics Singapore Pte Ltd

0 件の賞賛
返信

2,292件の閲覧回数
sinanakman
Senior Contributor III

Hi Arun

Freescale has a replacement probe called CWTAP that

you should be able to use with MPC8640.

We are using a Abatron BDI3000 probes here.

Hope this helps

Regards

Sinan Akman

0 件の賞賛
返信