MPC855T versus MPC860DP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC855T versus MPC860DP

1,006件の閲覧回数
steven_keeter
Contributor I

Is the MPC860DP pin for pin compatible with the MPC855T?  The MPC855T is now on LTB, but the MPC860DP still is ACTIVE.  Basically I need to replace the MPC855T with either a drop-in equivalent or do a PCB spin and port the code to the next closest variant.  Can someone please give me advise on this?  Also, if the MPC860DP can be used, how long will it be available?

 

Thanks

タグ(1)
0 件の賞賛
返信
0 返答(返信)