MPC8548E : PCB Layout Guidelines for Local Bus Interface signals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8548E : PCB Layout Guidelines for Local Bus Interface signals

Jump to solution
3,445 Views
sagar_bn
Contributor I

Please provide PCB Layout guidelines for Local Bus interface signals of MPC8548E.

Should we follow any length matching for LAD[0:31] signals ?

Please also let us know about all the local bus interface signals for which layout guide has to be followed.

Tags (1)
0 Kudos
Reply
1 Solution
3,431 Views
yipingwang
NXP TechSupport
NXP TechSupport

No general document is avialable. What is the device intended for interfacing?

Maybe some Freescale evaluation boards can be referred.

View solution in original post

0 Kudos
Reply
3 Replies
3,424 Views
sagar_bn
Contributor I

We are using Local Bus Interface of MPC8548E for interfacing with many devices like NOR Flash, NAND Flash, NVSRAM, and two FPGAs.

These signals are running throughout my VPX standard board because of multiple components at different locations.

Please share if any Evaluation board file available.

0 Kudos
Reply
3,336 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please find attached 8548CDS board design material. All people generated this files are gone. It is prepared by Mentor Graphics and it is not Cadence that board team are using. Simple put, no support for this file.

Alternatively, please refer to P4080DS material local bus design if the customer cannot make use of 8548 file.

0 Kudos
Reply
3,432 Views
yipingwang
NXP TechSupport
NXP TechSupport

No general document is avialable. What is the device intended for interfacing?

Maybe some Freescale evaluation boards can be referred.

0 Kudos
Reply