MPC8548E Memory Map CCSR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8548E Memory Map CCSR

2,076 Views
axlmr
Contributor I

I have a question about the  CCSR Register

In the documentations says

All of the memory mapped configuration, control, and status registers in the MPC8548E are contained

within a 1-Mbyte address region. To allow for flexibility, the configuration, control, and status block is

relocatable in the local address space.” ‘Section 2.3 Reference Manual.

What is the process to relocate this register? When and How it is done?

1 Reply

1,601 Views
scottwood
NXP Employee
NXP Employee

The process is documented in the "Updating CCSRBAR" section of the manual (4.3.1.1.1).  It is typically done during early boot if the default address isn't desired (e.g. if you want to use 4GiB or more of RAM, you'll want to move CCSR out of the way).  U-Boot has code to relocate CCSRBAR in arch/powerpc/cpu/mpc85xx/start.S.