MPC8548CDS Qemu U-boot Ethernet Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8548CDS Qemu U-boot Ethernet Issue

1,622 次查看
pbasvat
Contributor I
Hi, I am trying to simulate mpc8548 powerquic processor using qemu as i don't have any boards with me. but while trying to simulate i am facing issue of ethernet interface at u-boot level. Below are steps i have used for qemu source compilation & u-boot cross-compilation for mpc8548 hw. Qemu compilation for powerpc # ./configure --prefix=/home/pbaswat/TechnicalWS/QUEMU/install_dir/ --target-list=ppc-softmmu,ppc64-linux-user,ppc-linux-user,arm-softmmu,arm-linux-user --enable-debug --disable-strip --disable-werror # make && make install U-boot cross-copilation 1) # export LD_LIBRARY_PATH=/opt/PPC/cross-tools/lib/ 2) # make ARCH=powerpc CROSS_COMPILE=powerpc-unknown-linux-gnu- MPC8548CDS_config 3) # make ARCH=powerpc CROSS_COMPILE=powerpc-unknown-linux-gnu- qemu powerpc launch command # sudo qemu-system-ppc -M ppce500 -m 1024M -nographic u-boot.bin -device e1000 -net nic -net tap,ifname =vnet0,script=no,downscript=no ------------------------------------------------------------------------------------------------------------------------------------------ $ sudo qemu-system-ppc -m 1024 -M ppce500 -nographic u-boot.bin -device e1000 -net nic -net tap,ifname=vnet0,script=no,downscript=no ----------------------------------------------------------------------------------------------------------------------------------------- U-Boot 2019.01 (Mar 04 2019 - 11:07:45 +0100) CPU: Unknown, Version: 0.0, (0x00000000) Core: e500, Version: 3.0, (0x80210030) Clock Configuration: CPU0:400 MHz, CCB:400 MHz, DDR:200 MHz (400 MT/s data rate), LBC: unknown (LCRR[CLKDIV] = 0x00) L1: D-cache 32 KiB enabled I-cache 32 KiB enabled DRAM: 1 GiB L2: disabled PCI: base address e0008000 00:01.0 - 1af4:1000 - Network controller 00:02.0 - 8086:100e - Network controller PCI1: Bus 00 - 00 In: serial Out: serial Err: serial Net: guts: Unknown register read: 8 guts: Unknown register read: 8 guts: Unknown register write: d8 = ffffffff guts: Unknown register write: 100 = 0 guts: Unknown register write: 400 = 8000000 guts: Unknown register read: 8 guts: Unknown register read: 0 guts: Unknown register write: 0 = 4 guts: Unknown register write: d8 = ffffffff guts: Unknown register read: c0 guts: Unknown register read: 10 guts: Unknown register read: 8 e1000: 00:00:00:00:00:00 e1000#0 Error: e1000#0 address not set. Hit any key to stop autoboot: 0 =>
标记 (1)
0 项奖励
回复
2 回复数

1,606 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I need to discuss this issue with the AE team, will provide feedback later.

0 项奖励
回复

1,586 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following update from the AE team.

We support QEMU to boot Linux kernel, but nobody has verified booting uboot. I think you can let customer know. It looks like that  their purpose is to boot Linux, so they don't have to boot uboot. Please check out LSDK UM, ch 10.

0 项奖励
回复