MPC8548 when reads the data from the PCIE is and to write into the DDR2 CPU core intervention is required or not?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC8548 when reads the data from the PCIE is and to write into the DDR2 CPU core intervention is required or not?

1,191 次查看
lakshmit
Contributor I

PC8548 when reads the data from the PCIE is and to write into the DDR2 CPU core intervention is required or not?

0 项奖励
回复
1 回复

1,128 次查看
ufedor
NXP Employee
NXP Employee

The CPU intervention is not required - i.e. PCI Express transactions targeting MPC8548 inbound ATMU with translation to a DDR2 SDRAM region are converted to direct memory read/write operations by the PCI Express interface.


Best regards,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复