MPC8548 Problem with Jumbo Packets

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8548 Problem with Jumbo Packets

2,446件の閲覧回数
diegomartin
Contributor I

Hello!!

I have a problem sending larges UDP messages with a MPC8548.

After configuring all registers properly (i think), when i send a message with more than 2005 bytes, the message doesnt reache the PC who is waiting for.

I had to change the value of the following registers for this:

  - MAXFRM = 0x00002580 (9600 bytes)

 - MACCFG2 =0x00007105

 - Flags of packet: 0xBA82 (WRAP), 0x9A82 (without WRAP)

Any idea?

Thank you in advance,

Diego.

ラベル(1)
0 件の賞賛
返信
1 返信

2,354件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the eTSEC 55 chip erratum:

https://www.nxp.com/docs/en/errata/MPC8548ECE.pdf

 

See also the Table 14-38 in the Errata to MPC8548E Reference Manual, Rev. 2:

https://www.nxp.com/docs/en/reference-manual/MPC8548ERMAD.pdf

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信