MPC837x PCIe sample embedded driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC837x PCIe sample embedded driver

1,284 Views
tuyen_nguyen
Contributor I

I start writing PCI Express driver code for the embedded system in which master embedded board is using MPC837x to communicate with other devices using PCIe . I have no experience in such driver and do not know where to start. Anyone can provide or point me to where I can find the basic PCIe driver of this processor MPC837x or similar one? Thanks

0 Kudos
Reply
1 Reply

1,223 Views
ufedor
NXP Employee
NXP Employee

Please refer to the U-Boot PCI driver source code and PCIe patches provided in the MPC837x MDS LTIB BSP:

LTIB BSP for MPC837x MDS 

0 Kudos
Reply