MPC8379E core power consumption.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8379E core power consumption.

963 Views
saravanakumar_s
Contributor I

What shall be the power consumption of the core of  MPC8379E (667Mhz) processor typically and maximum?. To design the 1.0V regulator for core supply.

0 Kudos
Reply
1 Reply

907 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

The estimated typical power dissipation for the chip device is shown in Table 5. Power Dissipation of the MPC8379E PowerQUICC II Pro Processor Hardware Specifications, Rev. 10. You can download it from the Freescale page

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC8379E

For core frequency 667MHz and CSB/DDR frequency 333MHz Typical is 2.1W (T=65’C) and Maximal is 4.1W (T=125’C)

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply