MPC8378E about DUART, how many size(1 byte?) of the transmit and receive buffer of the DUART?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC8378E about DUART, how many size(1 byte?) of the transmit and receive buffer of the DUART?

跳至解决方案
1,938 次查看
dennisxie
Contributor I

Hi, guys

I meet some issue of MPC8378E DUART interface.

My question:

MPC8378E about DUART, how many size(1 byte?) of the transmit and receive buffer of the DUART?

wait for you reply. Thanks

Dennis Xie

2015.11.18 China Beijing

0 项奖励
回复
1 解答
1,827 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

In FIFO mode for both transmitter and receiver, the MPC8378 UART has 16-byte FIFOs

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,827 次查看
dennisxie
Contributor I

Hi

How is the last question, still wait for your reply.

Here I have another question more:

1)for FIFO-mode and none FIFO mode, how to distinguish the FIFO/URBR/UTHR?  seems the URBR and UTHR have same offset(0x4500/0x4600).

2)in FIFO mode,  is the URBR/UTHR be the come in and go out base address?

3)if there are both send and receive FIFOs, then how is the FIFOs connect to the URBR and UTHR?

Wait for you reply! Thanks!

Dennis

2015.12.01  China Beijing

0 项奖励
回复
1,828 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

In FIFO mode for both transmitter and receiver, the MPC8378 UART has 16-byte FIFOs

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,827 次查看
dennisxie
Contributor I

HI, thanks, I meet another problem:

when the IID3–IID0 is 1100(Character time-out), what's the meaning of this Interrupt Description

No characters were removed from or input to

the receiver FIFO during the last four

character times and at least one character is

in the receiver FIFO.

every time I open duart driver to read the RX buffer in fifo mode, I will flush the RX fifo(write the 0x4602 with 0xC3), how could it can receive one character, it is so strange, would you help this???

Wait for your reply. Thanks.

Dennis Xie

2015.11.25 China Beijing

0 项奖励
回复