MPC8377 MVREF Design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8377 MVREF Design

2,089件の閲覧回数
sollong-gos
Contributor I
I designed and manufactured the SBC board using the MPC8377.
Sometimes memory errors occur at low temperatures (less than -30 degrees Celsius) and the system is not booting normally and can not boot
Q) When 200 ohms is not applied to MVREF, can this cause the phenomenon?
ラベル(1)
  • DDR

0 件の賞賛
返信
1 返信

1,939件の閲覧回数
Bulat
NXP Employee
NXP Employee

I can not know what is exact reason of your temperature issue, however the "Design checklist" (AN3665) directly states: "Each of the MVREF1 and MVREF2 supply inputs must be connected through serial resistors of 200 Ohm." We strongly recommend to follow this requirement.

Regards,

Bulat

0 件の賞賛
返信