MPC8377 MVREF Design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8377 MVREF Design

2,139 Views
sollong-gos
Contributor I
I designed and manufactured the SBC board using the MPC8377.
Sometimes memory errors occur at low temperatures (less than -30 degrees Celsius) and the system is not booting normally and can not boot
Q) When 200 ohms is not applied to MVREF, can this cause the phenomenon?
Labels (1)
0 Kudos
Reply
1 Reply

1,989 Views
Bulat
NXP Employee
NXP Employee

I can not know what is exact reason of your temperature issue, however the "Design checklist" (AN3665) directly states: "Each of the MVREF1 and MVREF2 supply inputs must be connected through serial resistors of 200 Ohm." We strongly recommend to follow this requirement.

Regards,

Bulat

0 Kudos
Reply