MPC8355 DDR2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8355 DDR2

1,356 Views
WWWA_YURI
Contributor I

I try to set the DDR control registers of the MPC8533.
Please tell me how to decide the setting values of the following registers.

1. DDR SDRAM Data Initialization (DDR_DATA_INIT)
2. DDR Initialization Address (DDR_INIT_ADDR)
3. DDR Initialization Enable Extended Address (DDR_INIT_EXT_ADDR)

0 Kudos
Reply
1 Reply

1,324 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. DDR SDRAM Data Initialization (DDR_DATA_INIT)
this is the value that will be written to the DDR2 after initialization has completed if D_INIT bit is set before MEM_EN is set. the value in this register is not very important, it is to initialize the DRAM DDR2 mostly useful when ECC is enabled.


2. DDR Initialization Address (DDR_INIT_ADDR)
3. DDR Initialization Enable Extended Address (DDR_INIT_EXT_ADDR)

the above two registers is most of time is left at zero. this is the starting address of 128 byte, that will be used by the controller to perform the DDR initialization

0 Kudos
Reply