MPC8349E Clock Connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8349E Clock Connection

2,459 Views
youngho_cho
Contributor II

Dear MPC8349E expert,

I'm going to use MPC8349E processor for main processing unit on the new project.

I'm confused about the clock connection.

To provide information about our system, processor e300 core frequency grade is AL(667MHz), platform frequency is 333MHz, and CSB frequency will be 333MHz, as well local bus frequency will be 133MHz, and we will not use PCI port.

In this case, according to MPC8349EEC or MPC8349EARM, connecting the clock to 66MHz or 66.67MHz is mixed. I wonder if I should connect to the 66MHz or 66.67MHz option.

I look forward to your kind response.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

2,451 Views
r8070z
NXP Employee
NXP Employee

You can apply up to 66.67MHz - minimal  CLKIN/PCI_CLK cycle time is 15 ns.

 

0 Kudos
Reply