MPC8349E Boot ROM and Reset Configuration Words

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8349E Boot ROM and Reset Configuration Words

1,512 Views
youngho_cho
Contributor II

I am considering using parallel NOR flash connected through local bus GPCM for storing MPC8349E's booting image and reset configuration words.

According to the reference manual, there are examples of EEPROMs for storing the boot ROM and reset configuration words.

I wonder if I must use the EEPROM or if I can use the equivalent nonvolatile memory, such as the aforementioned NOR flash.

Tags (2)
0 Kudos
Reply
1 Reply

1,502 Views
ufedor
NXP Employee
NXP Employee

Parallel NOR Flash can be used.

Please refer to the MPC8349EA PowerQUICC II Pro Integrated Host Processor Family Reference Manual, 4.3.2 Reset Configuration Words:

"The reset configuration words are loaded from the local bus or from the I2C interface or from hard-coded values during the power-on or hard reset flows."

4.3.1.1 Reset Configuration Word Source:

CFG_RESET_SOURCE[0:2] = 000  (Reset configuration word is loaded from a local bus EEPROM.)

4.3.3.1 Loading from Local Bus EEPROM

0 Kudos
Reply