MPC8323 File system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC8323 File system

1,984件の閲覧回数
vadrevujyothi
Contributor I

Hi,

       I am using MPC8323E-RDB Board with U-Boot 1.1.6 version and kernel 2.6. I want to load flash file system but in Data sheet only Ramdisk file system mentioned. I am trying to load jffs2 file system into flash but it is not at all writing into flash. Can i load flash file system in MPC8323 board and i want to store some data files in flash at run time according to my application requirement. Can you suggest Which file system i have to use for my requirement and how can i load that into my board?

タグ(1)
0 件の賞賛
返信
1 返信

1,819件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at attached file. It is LTIB User's Manual for the MPC8349 boar. Find the "JFFS2 Deployment" in this file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信