MPC8323 File system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC8323 File system

1,392 Views
vadrevujyothi
Contributor I

Hi,

       I am using MPC8323E-RDB Board with U-Boot 1.1.6 version and kernel 2.6. I want to load flash file system but in Data sheet only Ramdisk file system mentioned. I am trying to load jffs2 file system into flash but it is not at all writing into flash. Can i load flash file system in MPC8323 board and i want to store some data files in flash at run time according to my application requirement. Can you suggest Which file system i have to use for my requirement and how can i load that into my board?

Tags (1)
0 Kudos
Reply
1 Reply

1,228 Views
Pavel
NXP Employee
NXP Employee

Look at attached file. It is LTIB User's Manual for the MPC8349 boar. Find the "JFFS2 Deployment" in this file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply